STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stacking IHM06A1

Posted on May 14, 2018 at 11:29I'm hoping someone can provide a straight-forward answer as to how I can operate multiple stepper motors using stacked IHM06A1 boards. In example code, the STSpin220 class is initialised as motor = new STSpin220(D2, D8...

Resolved! what is the best IDE? Keil or Eclipse or Atollic Studio?

Posted on May 13, 2018 at 10:46Hi Team,I am new to STM32 MCU family. I have with me no STM32F04 Discovery board.To get started what is the best IDE? Is keil good or eclipse good or Atollic studio is good?  with out nay code size limitations.Kindly s...

Trying to put STM32L471RG into Shutdown mode

Posted on December 13, 2016 at 09:52I am trying to put the STM32L471RG into Shutdown mode.I am doing the following steps, based on the documentation.// Turn on Deepsleep bit SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk | SCB_SCR_SLEEPONEXIT_Msk; // Setup Low P...

Unable to set up USART2 on NUCLEO-L432KC: assert_param failure in stm32l4xx_hal_uart.c and/or call to HardFault_Handler.

Posted on May 13, 2018 at 06:07 Hello, I have a NUCLEO-K432KC. In a STM32CubeMX project, I ensured USART2 and GPIOB3 were enabled per the manual. I2C1 is also enabled. A full project can be seen at https://github.com/R030t1/stm32-touchpad. ...

Discovery B-L475E-IOT01 to Nucleo 144 porting

Posted on May 14, 2018 at 09:06Hi Im trying to port B-L475E-IOT01 applications to Nucleo144 L4RZI. Im facing issuing on porting the driver. UART,SPI,I2C. Im strange to see that the data is not being pumped out of COM Port, while in debug the data bu...

Resolved! Failed to Download stm32cubeh7.zip ...

Posted on May 14, 2018 at 04:43As usual, I've tried to download stm32cubeh7.zip but it failed due to the network error.I couldn't download via FlashGot or any resumable download tool. Does any one have a mirror of the stm32cubeh7.zip?In addition, do...

bnarit by Associate II
  • 1152 Views
  • 2 replies
  • 0 kudos

Nucleo 144 BSP

Posted on May 13, 2018 at 21:19Hi, I am looking for bsp in keil for nucleo144 board but i am not able to find it in the latest version of the keil. Where can i find the bsp for the same? What is the procedure?

Need the code of the adc for a stm32f3

Posted on May 13, 2018 at 22:00hello everyone ,please I try to get a voltage in the pin PA0 of a stm32F3 DISCOVERY and convert it with the adc of this pin and display it on system workbench, but I need a code on the software Basic workbench system t...

STM32F3 simultaneous ADC conversions

Posted on May 09, 2018 at 12:54Hi.I want to do do ADC conversions on all 3 ADCs simultaneous: they should be done in the same time. How should I achieve that?1. With DMA? I can do multichannel conversions, but they are not simultaneous. When I start...