cancel
Showing results for 
Search instead for 
Did you mean: 

I2C Bug in STM32CubeF2 Firmware Package V1.4.0

Posted on December 05, 2016 at 17:45

Hi folks,

my application crashes occasionally with the above mentioned firmware package when data is transmitted to I2C devices.

The crash is caused by following code in HAL_I2C_Master_Transmit:

    while(hi2c->XferSize > 0U)

    {

      /* Wait until TXE flag is set */

      if(I2C_WaitOnTXEFlagUntilTimeout(hi2c, Timeout, tickstart) != HAL_OK)

      {

           ...

      }

      /* Write data to DR */

      hi2c->Instance->DR = (*hi2c->pBuffPtr++);

      hi2c->XferCount--;

      hi2c->

XferSize

--;

      if((__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_BTF) == SET) && (

Size

!= 0U))

      {

You can get here when

I2C_FLAG_BTF

is set due to delay (interrupt) and

XferSize

== 0 because the wrong var (

Size

) is checked. This results in

XferSize

wrapping around to 0xffff. The transmit loops continues and usually the

pBuffPtr

runs beyond bounds causing a bus error.

        /* Write data to DR */

        hi2c->Instance->DR = (*hi2c->pBuffPtr++);

        hi2c->XferCount--;

       

hi2c->XferSize--;

      }

This code fragment can be found several times in stm32f2xx_hal_i2c.c.

I temporarily went back to Rev 1.3.0.

Christian

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Walid FTITI_O
Senior II
Posted on December 06, 2016 at 11:29

Hi

backeberg.christian

,

Thank you for the feedback and contribution. I send internally your request for check.

-Walid FTITI-

Posted on October 18, 2017 at 14:58

Hi Walid,

recently I noticed an update of stm32f2xx_hal_i2c.c to revision 1.6.

I checked it against the above mentioned bug.

It seems that the bug has not being fixed in all places were it can occur.

In HAL_I2C_Slave_Receive() at Line 1142 the old code can be found.

Christian

Posted on October 18, 2017 at 16:18

Hi

backeberg.christian

‌,

Thanks for highlighting this again, this will be reviewed and fixed.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on February 01, 2018 at 17:19

Sorry, but the above mentioned bug is still not fixed in Rev 1.7.0.

Line 1140:

      if((__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_BTF) == SET) && (Size != 0))

should be:

     if((__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_BTF) == SET) && (hi2c->XferSize != 0))

Greetings - Christian