STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 ADC speed

Posted on September 21, 2017 at 19:46Hello,the STM32H753bi.pdf datasheet Rev1 tells on page 2:3× ADCs with 16-bit max. resolution (14 bits2.7 MSPS, 16 bits 168 kSPS)This would imply a 14-bit SAR adc and 16 bit as a result of oversampling.In chapter...

APB1ENR Power interface clock enable bit

Posted on June 07, 2018 at 09:36I am using stm32F0 and Stm32L0 series MCUs.APB1ENR in Stm32 has Power interface clock enable bit (Bit 28). I have gone through the reference document to unserstand what is its significance.  Bit 28 PWREN: Power interf...

STEVAL-3DP001V1

Posted on June 07, 2018 at 12:45i bought the STEVAL-3DP001V1 for printer 3d last mouth. i got problem with wifi. the webserver not work.it can connect wifi and display. but it can not response any function to the stm chip.  i can't change the ssid a...

Anh Vu by Associate II
  • 771 Views
  • 0 replies
  • 0 kudos

Bug in STM32CUBEMX 4.26

Posted on June 07, 2018 at 09:32Hello,i have updated STM32CubeMx from 4.25.1 to 4.26 and now i can no more generate my project. It freezes during the generation project. I uses a STM32L475.ST, please give me a link to download the 4.25.1 version bec...

Memory read out protecion STM32F407IGX

Posted on June 06, 2018 at 15:57STLing is showing error (memory in read out protection). Cannot get access to memory even via DFU (DFuSe, Flash loader demo, via USB OTG FS or USART3(PC10,PC11) with PC2102). First time i did get access via USB and DF...

Resolved! About STM32L1 IBIS Model name

Posted on June 06, 2018 at 12:45Hello.I wanna ask that I don't know about the filename of IBIS about STM32L1.I download it from the product page, it looks like:I don't understand what ''429/427/436'' is.I googled that it's about STM32F1XXX or other,...

0690X0000060BYwQAM.png

Cannot read config register value of M24LR16E via I2C

Posted on June 07, 2018 at 09:34Hi All,I'm trying to communicate with M24LR16E(NFC tag IC) via I2C (STM32F103R is Master)I could find configuration register(address 2320) has initial value 0xF4.so I tried to read the configuration register, but I go...

Resolved! STM32 RTC miliseconds set

Posted on May 14, 2018 at 19:40Hi,I would like to set the milliseconds in the STM32 RTC, the function hal_rtc_settime doesn't change the milliseconds (subseconds) value.I tried be setting hrtc->instance->rtc_ssr but it doesnt change its valueHelp wo...

priven by Associate II
  • 4014 Views
  • 8 replies
  • 0 kudos

Reset MCU?

Posted on June 03, 2018 at 13:12Hi,i am beginner in stm i am working on stm32l071, have configured rtc,spi,uart all peripherals working good,butsome time MCU resetting how to find what is reason for resetting  the mcu.