STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 RTC miliseconds set

Posted on May 14, 2018 at 19:40Hi,I would like to set the milliseconds in the STM32 RTC, the function hal_rtc_settime doesn't change the milliseconds (subseconds) value.I tried be setting hrtc->instance->rtc_ssr but it doesnt change its valueHelp wo...

priven by Associate II
  • 4027 Views
  • 8 replies
  • 0 kudos

Reset MCU?

Posted on June 03, 2018 at 13:12Hi,i am beginner in stm i am working on stm32l071, have configured rtc,spi,uart all peripherals working good,butsome time MCU resetting how to find what is reason for resetting  the mcu.

Low power mode power consumption gpio pin low

Posted on June 07, 2018 at 04:35Hello,When I enter low power mode, I need to pull all gpio pin to LOW?To pull gpio low can make mcu power current low?Is there any doc about how to measure the power current in low power mode?Thanks

cyt by Associate II
  • 763 Views
  • 1 replies
  • 0 kudos

STm32F3 discovery kit Problem

Posted on June 06, 2018 at 23:52hello,i wanted help for the STM32F303. Initially when i was 'Turning on' the STM32F303 Kit the leds start displaying but now they are neither blinking nor and leds are showing direction of North.How can i bring or res...

STLinkv2.1 comm error for SWD on STM32469I-Eval

Posted on June 07, 2018 at 07:49Hi,I have STM32469I-Eval board.I used STM32SW4 (AC6) toolchain and built a LED toggle project and debugged it using OpenOCD.Everything was working good.Then i did HW modifications on it by removing CN2, CN4, R216, R21...

STM32429 CAN bus Transmitt Mailbox not trasnmitting?

Posted on June 07, 2018 at 00:42I'm trying to implement the sample code \stm32cube_fw_f4_v1210\STM32Cube_FW_F4_V1.21.0\Projects\STM324x9I_EVAL\Examples\CAN\CAN_Networking\Src on a STM32F429 Nucleo board. Using CubeMx. Single board for now. No transc...

kaveh k by Associate II
  • 3917 Views
  • 5 replies
  • 0 kudos

STM32F7 QSPI Erase and Write (with DMA) Too Slow

Posted on June 07, 2018 at 04:00Hi, all,I have already implemented the configuration of QSPI working in QUAD mode, and DMA2. I want to ready and write about 15M Byte data with QSPI flash. The time cost for reading data is about 2s. However, the time...