STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32f303CCT problem for reading TI's ADS1299

Posted on June 13, 2018 at 08:33When I try to read from ADS 1299 by using read command. The data sent by ADS 1299 is loaded into SPI data register of stm32f303 but sometimes it appears in lower 8 bits and some times in upper 8 bits.

Resolved! A question about Demo software come with demo board?

Posted on June 13, 2018 at 01:31Hello, I went to STM32 IoT discovery Kit seminar last year at San Francisco. At that time, I received a demo board (STM32 IoT Discovery Kit) with a USB memory card. Recently we have a project may need this MCU, and I ...

STM32F746 timer generated trigger for ext. ADC

Posted on June 12, 2018 at 11:33Dear STM32 timer specialists,i have to design a board, where a STM32F746 must read a 16 bit/40MSample ADC, into internal or external (SD)RAM. The ADC data bus will be 32 bit wide with 20MHz clock. The memory interface...

[STM32L0:SPI] Hard output NSS

Posted on June 08, 2018 at 17:31Hi,I'm trying to use the hardware controled NSS pin, but I'm getting some trouble.According to the Reference Manual:'The NSS signal is driven low as soon as the SPI is enabled in master mode (SPE=1), and is kept low u...

Searching for a 2 CAN board

Posted on June 12, 2018 at 09:44 Hello everyone, I am looking for a board with a STM32F4 or any other microcontroller (STM32) with 2 CAN. The main issue I am facing, is finding a developpement board where the 2 CAN inputs/outputs are available (f...

B C by Associate II
  • 2970 Views
  • 12 replies
  • 0 kudos

Turns itself PWM on STM32F030F4

Posted on April 27, 2018 at 07:49Hello. Dear forum users, help to understand the problem of the incorrect operation of the PWM control program. I'm writing on HAL in KEIL v5 environment, the signals are monitored by the analyzer. The problem is this...