STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Audio In & Out

Posted on June 08, 2018 at 17:43The original post was too long to process during our migration. Please click on the attachment to read the original post.

marek2399 by Associate II
  • 3692 Views
  • 6 replies
  • 0 kudos

Can bus problem

Posted on June 10, 2018 at 15:55Hello  everyoneI am using stm32f429 discovery board. I run CAN hal_lib example( networking ) and monitored tx pin on oscilloscope and got bellow signal( it is attached)I know the can frame, but the signal that is capt...

Amir Amir by Associate II
  • 2542 Views
  • 4 replies
  • 0 kudos

A suggestion on a gsm and gps module

Posted on June 12, 2018 at 11:26A customer requires a module, with a stm32 microcontroller, that can connect to a remote server to send data.I need a low cost gsm uart module that can connect to internet, to establish a tcp connection with a remote ...

Problem with SPI_SLAVE_DMA transmision

Posted on June 11, 2018 at 18:29hi stI have problem using spi slave with dmai use stm32f746 as slave to transmit data to master pc i send for test fixed frame start with check char ''$>'' to sync timing then slave should send 12 bytes ( 1-12)problem...

0690X0000060LDDQA2.png
egywell by Associate II
  • 713 Views
  • 2 replies
  • 0 kudos

FMC synchronous PSRAM - lost AHB transactions

Posted on October 30, 2017 at 14:09 Hello I have FPGA with memory mapped peripheral what I would like to control from external STM32 MCU (STM32F767 ). I chose FMC peripheral in synchronous PSRAM mode because communication can be easily impleme...

dstindl9 by Associate II
  • 14348 Views
  • 16 replies
  • 0 kudos

SPI Slave missing interrupts (NUCLEO-F401RE)

Posted on June 12, 2018 at 11:11Hi,im trying to implement a basic SPI full-duplex slave using HAL (the reason to use HAL here is that i have to switch to another STM MCU later).The biggest problem is that the slave sometimes doesn't seem to react to...

0690X0000060LDwQAM.png 0690X0000060LE1QAM.png 0690X0000060LEQQA2.png 0690X0000060LEVQA2.png
F. Pabst by Associate
  • 808 Views
  • 0 replies
  • 0 kudos

Slow Clock at powerup requires reset each time

Posted on June 08, 2018 at 20:57Hello,   I'm having an odd time with a board using the STM32F746VGT6 microcontroller that it requires that I reset the board each time that I power it up.  I have several of these and the phenomenon only occurs on abo...

Resolved! NUCLEO-F429ZI - SDIO - FatFs Problem

Posted on June 11, 2018 at 09:56Dear All, I’m new to this forum and to stm32 board. I’m trying to connect an SD Card to my board NUCLEO-F429ZI but I’m having some problems with it. I use STM32CUBEMX to create the project using the standard per...