User Activity

I would like to record/monitor a "3rd party" SPI bus conversation.I have a couple logic analyzers, that work fine on the bench.But i need longer term recording, and i need to do it in an environment without a PC and as small as i can get. And i am tr...
Posted on July 06, 2018 at 00:04I have a F446RE, with 5 devices connected to USART1,USART3,UART4,UART6,USART6In each case, i have DMA reception configured, each with decent size buffer.A have a 3 device versions, 2 work without issue, but model seem...
Posted on April 03, 2018 at 16:05I have read a few short posts around this forum, that suggest disabling a timer in PWM/OC mode, will change the output pins to high impedance.As background, I am trying to interface with a device that requires a PWM ...
Posted on February 15, 2018 at 16:02I can't remember the last time i could use a complete set of project files generated by CubeMX without having to patch something in the project that isn't user code.I am kind of tired maintaining backups of the pa...
Posted on October 27, 2017 at 16:34If you create a Cube project using the NUCLEO-F767ZI board template, it uses 16MHz for the HSE crystal.Out of the box, from the user manual, the dev board uses the:MCO from ST-LINK (Default): MCO output of ST-LINK ...
Kudos from