STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

usb fs cdc communication port

Posted on July 09, 2018 at 22:12I am using usb port nucleo f429zi. I know I need cdc library and I want to write some protocol (for example modbus) between usb and PC, so my program in PC can communicate with controller, is it possible to use IT to ...

yang hong by Associate III
  • 655 Views
  • 1 replies
  • 0 kudos

Why does CubeMX code for SystemClock_Config give error

Posted on July 10, 2018 at 01:10I am comparing an application project for stm32H7 with a project created from CubeMX that is meant to replicate the application project function.  The CubeMX project fails to run and I suspect a problem with the setup...

0690X0000060LdlQAE.png

Nucleo 144 Ethernet, LAN8742A, CubeMX 4.13.1?

Posted on March 17, 2016 at 20:35I needs some help.  I recieved a Nucleo 144 and I have used CubeMX 4.13.1 to generate some test code to try out the on-board ethernet.  Well I have had little success and cant seem to find the issue.  They come with ...

matthew23 by Associate II
  • 4363 Views
  • 6 replies
  • 0 kudos

Does anyone have an example project using IAP with VCP?

Posted on July 06, 2018 at 21:51Hi everyone,I'm trying to get IAP driver working on my STM32F072C8T6 with USB VCP. I saw an example code for STM32LX IAP projects with ymodem but I thought I would ask around first in case someone already has working ...

Justin K. by Associate II
  • 2753 Views
  • 5 replies
  • 0 kudos

Startup application for STM32F7 not working?

Posted on June 29, 2018 at 14:52We are using STM32F767ZIT6 Nucleo board and developing a startup application that jumps to the main application. The main application is a simple toggling LED app with a HAL_Delay API.By the below startup code we can ...

No-ST Link Detected in Nucleo-F767ZI

Posted on July 09, 2018 at 17:42Hello,I use Nucleo-F767ZI board as evaluation kit. Now, I faced a problem which is 'No-STLink device detected...'. When I connect the board with my laptop through USB cable, ST-link Firmware (version 2.31.21) does not...

AE104 by Senior
  • 695 Views
  • 0 replies
  • 0 kudos

DMA MEN2MEN and DMAMUX

Posted on July 06, 2018 at 11:29Hello,is the DMAMUX somehow involved when doing DMA MEM2MEM transfers? Is the value in the DMAMUX channel corresponding to the selectedMEM2MEM DMA channel irrelevant or must it be zero? I did not see MEM2MEN mentioned...

How to play video on the stm32 ?

Posted on July 09, 2018 at 07:37Hello everyone, I want to start a project. I will play video with stm32 in this project. How can I play video ? please help me ? Thanks.

STM32F746 low-layer driver issue: ADC DMA TIM2 trigger

Posted on July 05, 2018 at 16:49Dear Community,I am trying to migrate some code of a STM32F4 series µC relying on the StandardPeripheralLib to STM32F7 “low layer� driver concept. Unfortunately the LL-Driver concept is not that identical to Stan...

M G_2 by Associate III
  • 2405 Views
  • 3 replies
  • 0 kudos