STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 peripheral screen

I'm trying to write to the on-board peripheral screen of the STM32F429I board, but haven't found a working example: I tried following along some examples online and in the project directory, but they all reference functions like "HAL_Init()" or "BSP_...

Resolved! RM0433 and devices header disagree on BDMA registers

RM0433 talks about a BDMA_CM1ARx register and lists it in the register maps. The description in rm0433 for BDMA_CM1ARx seems to be tha same as for BDMA_CM0ARx. The device headers only talks about the CMAR register.Please clarify.

brightness of the led connected to the stm ic pin reduces.

Hai I have a simple design.I am using STM32F051R4T6TR.I just connected a led such that the led sinks the 20mA current when the led turns on.i happen to notice that each time i switch on my board the brightness of my led is getting reduced.this happen...

Amal Babu by Associate III
  • 2083 Views
  • 5 replies
  • 0 kudos

Execution of code in SRAM of STM32F405

Hi, I am using STM32F405.I use the Flash Sector as follows. - Sector 0: IAP - Secotr 2: Data Save - Sector 5: Main ApplicationMain Save the data in APP. And Main_APP erases Sector2 before writing the data.While erasing Sector2 from Main_APP, I notice...

JPark.18 by Associate
  • 1035 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F030RC programming flash problem

HiI have used STM32F030RC.I program the flash memory, using bootloader from PA9 and PA10.I have programmed the microcontrollers first time successfully. But after some program times, I can not program them. I traced the problem. The micro goes to b...

C++ IDE?

Posted on April 10, 2018 at 06:06Anyone has ever tried to install and play with an C++ arduino oriented  IDE that uses arduino libraries but implemented for STM32 micros?Have you ever heard of Sloeber?http://eclipse.baeyens.it/ Seems interesting!

g. lewis by Associate II
  • 8707 Views
  • 22 replies
  • 0 kudos

Nucleo F767ZI - system freeze upon UART ORE interrupt

Hi,My system (MCU) gets into a state where I can't debug it when i get a UART interrupt due to ORE.I even tried placing breakpoints at the places where ORE is captured in the IRQ handler - but the debugger didnt stop and I lost the connection to the ...