User Activity

I am running RTC for stm32h753. If I read the time of RTC, I do not get updated value as shown in below example. I am using LSE 32.768Khz. As it can be seen that 00:08:10  is being read repeatedly and then 00:08:15. if I compare overall time, it is ...
Hi, cube programmer does not reset the board after loading finished and board remains in boot loader mode. Older Dfuse demo utility used to reset board after loading finished. Does any one has some idea to reset the board grammatically and bring out ...
Hi, I am trying to use Stm32 cube programmer with stm32h753 in USB dfu mode. Moving the mcu in boot loader mode and usb is appearing , when I press the connect button it gives this error 23:42:46:012 : Error: Data read failed23:42:46:170 : Warning: C...
Hi,Does ST have any Mcu with 32-bit lptimer or 32-bit wakeup timer ?Or there is any plan to do that in near future :)Thanks,
Hi, I have configured two 16-bit general purpose timers in master slave mode and made 32 bit timer to get the time base ranging from micro seconds to minutes. I want to configure two 16-bit LP timers to wake up the system after for specified time ran...
Kudos from