cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to read the all sensors values at once L475E-IOT01

Tech world
Associate II
Posted on April 23, 2018 at 09:33

Hi everyone,

I am using STM32L475 B-L475E-IOT01 kit. My problem is that it does not give me sensors values at once. I want to get the temperature, humidity, pressure, accelerometer and gyro at once. But it only gives me 4 sensor values at once. For example, I have to comment out my one of the sensor code then it gives me the sensor values otherwise when I load my code into the kit with 5 sensors code then the user LED is not blinking. There is no error in the code. I run the code for every sensor individually to get the values and it gives me the values.  Please help me with this problem.

thank you

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on April 23, 2018 at 22:02

I don't use that kit, but I guess the code which comes with it is whipped together from portions of Cube with a pinch of FreeRTOS; and that it simply overflew the m�gic pot. Hardly is there an instant solution.

when I load my code into the kit with 5 sensors code then the user LED is not blinking

Maybe start with finding out, exactly why the LED is not blinking.

JW