STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F030F4P6 with Arduino IDE or Atmel Studio

Hello,I have just got a new board that I purchased using the STM32F030F4P6 MCU.This is a Mini Developing board that you can get from Ali Express and it is good as well IMHO.The Board that I have is:And I am bit struggling to make it to work under Ard...

0690X000006C5ywQAC.jpg
AGUET by Associate II
  • 6643 Views
  • 5 replies
  • 0 kudos

STM32F0 Communication with STPM33 Evaluation board

Hi All; I would like to measure active power. DataTx[0] = 0xFF; DataTx[1] = 0x00; DataTx[2] = 0xA0; DataTx[3] = 0x00; DataTx[4] = Metro_HAL_CalcCRC8(DataTx); HAL_SPI_TransmitReceive(&hspi1, (uint8_t *)DataTx, (uint8_t *)DataRx, sizeof(DataTx),10...

0690X000006CKqcQAG.jpg
Gz by Senior
  • 757 Views
  • 0 replies
  • 0 kudos

how to convert uint8_t to string

how to convert uint8_t to string and show in SSD1306_Putsi try like this.uint8_t check;SSD1306_Puts("choose dreep"+String(uint8_t), &Font_7x10, 1);

hande by Associate II
  • 3602 Views
  • 4 replies
  • 0 kudos

Question on TIM 1 interrupts

I would like to know more about the following interrupts so that I learn when to use them. Where can I find details about them?TIM1 Break interruptTIM1 Update interruptTIM1 trigger and commutation interrupt, specially this oneTIM1 Capture Compare in...

xpp07 by Senior
  • 832 Views
  • 1 replies
  • 0 kudos

STM32F769 Discovery touch panel part number for replacing it

Hello to everyone,recently I've got STM32F769I-DISCO board with B-LCD40-DSI1 that contains 4" LCD and touch panel. But it hasn't been a single day that I knocked over the board and broke the touch panel so it doesn't work now. So now I'm searching fo...

Alex Gab by Associate III
  • 2021 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F070F6 RTC Alarm is off by -15% when in Standby Mode

Hello,I'm using the RTC Alarm to wakeup the MCU every 10min and after 10PM, sleep for 10 hrs. However, I noticed that the RTC just actually sleeps for 8:25 min and when it wakes up, the RTC time says 10minutes have passed. To illustrate:Current time ...

Multiple ADC chanell on STM32L011K4T6 ?

Dear ST Forum Members,I'm experimenting with STM32L011K4T6 Nucleo,with ADC_LowPower Example project, I saw this :uhADCxConvertedValue = HAL_ADC_GetValue(&AdcHandle);If I want to use two channels of ADC, what should I modify,I've done ://ADCx Channel...