cancel
Showing results for 
Search instead for 
Did you mean: 

Can't send CAN message - Mailboxes always full

Miguel Antunes
Associate II
Posted on June 25, 2018 at 17:34

Hello,

I'm trying to configure the CAN-bus peripheral in loopback mode so I can later develop a real network. I'm using the Nucleo L432KC board and my clock is 32MHz.

My problem is that I can't send any messages andHAL_CAN_GetTxMailboxesFreeLevel() always returns 3 even without trying to send messages. Every time I try to send a message the code simply blocks and it does not enter the _Error_Handler() function. TheHAL_CAN_GetState() function returnsHAL_CAN_STATE_LISTENING.

I based my code on the example provided my ST in the HAL library (CAN_Networking).

Can you help me discovering what's wrong with this code?

Here is the CAN-bus configuration function:

static void MX_CAN1_Init(void)
{
 CAN_FilterTypeDef sFilterConfig;
 hcan1.Instance = CAN1;
 hcan1.Init.Prescaler = 8;
 hcan1.Init.Mode = CAN_MODE_LOOPBACK;
 hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
 hcan1.Init.TimeSeg1 = CAN_BS1_13TQ;
 hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
 hcan1.Init.TimeTriggeredMode = DISABLE;
 hcan1.Init.AutoBusOff = DISABLE;
 hcan1.Init.AutoWakeUp = DISABLE;
 hcan1.Init.AutoRetransmission = DISABLE;
 hcan1.Init.ReceiveFifoLocked = DISABLE;
 hcan1.Init.TransmitFifoPriority = DISABLE;
 if (HAL_CAN_Init(&hcan1) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 sFilterConfig.FilterBank = 0;
 sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
 sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
 sFilterConfig.FilterIdHigh = 0x0000;
 sFilterConfig.FilterIdLow = 0x0000;
 sFilterConfig.FilterMaskIdHigh = 0x0000;
 sFilterConfig.FilterMaskIdLow = 0x0000;
 sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
 sFilterConfig.FilterActivation = ENABLE;
 sFilterConfig.SlaveStartFilterBank = 14;
 if(HAL_CAN_ConfigFilter(&hcan1,&sFilterConfig) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 if(HAL_CAN_Start(&hcan1) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 TxHeader.StdId = 0x321;
 TxHeader.ExtId = 0x01;
 TxHeader.RTR = CAN_RTR_DATA;
 TxHeader.IDE = CAN_ID_STD;
 TxHeader.DLC = 2; //length
 TxHeader.TransmitGlobalTime = DISABLE;
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

Here is the RX interrupt handler:

void HAL_CAN_RxFifo0MsgPendingMessage(CAN_HandleTypeDef *hcan)
{
 HAL_GPIO_TogglePin(GPIOB,GPIO_PIN_3);
 if(HAL_CAN_GetRxMessage(hcan,CAN_RX_FIFO0,&RxHeader,RxData) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 if((RxHeader.StdId == 0x321) && (RxHeader.DLC == 2))
 {
 can_msg_received = 1;
 }
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

And here is part of the main code in which I try to send messages:

(...)
CAN_HandleTypeDef hcan1;
(...)
CAN_TxHeaderTypeDef TxHeader;
CAN_RxHeaderTypeDef RxHeader;
uint8_t TxData[8];
uint8_t RxData[8];
uint32_t TxMailbox;
(...)

int main(void)
{
 HAL_Init();
 SystemClock_Config();
 MX_GPIO_Init();
 MX_USART2_UART_Init();
 //MX_TIM2_Init();
 MX_I2C1_SMBUS_Init();
 MX_I2C3_Init();
 MX_CAN1_Init();
 (...)
 while (1)
 {
 millis = HAL_GetTick();
 if (millis-last_millis > 1000)
 {
 last_millis = millis;
 (...)
 TxData[0] = (uint8_t)((mymlx90614->IR_raw & 0xFF00) >> 8);
 TxData[1] = (uint8_t)(mymlx90614->IR_raw & 0xFF);
 return_value = HAL_CAN_GetState(&hcan1);
 while((return_value == HAL_CAN_STATE_READY) && (return_value == HAL_CAN_STATE_LISTENING));
 mailbox_level = HAL_CAN_GetTxMailboxesFreeLevel(&hcan1);
 sprintf(msg_send,'CAN Mailbox Level: %ld\r\n',mailbox_level);
 HAL_UART_Transmit(&huart2, (uint8_t*)msg_send, strlen(msg_send), 0xFFFF);
 if(HAL_CAN_AddTxMessage(&hcan1,&TxHeader,TxData,&TxMailbox) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 }
 if(can_msg_received == 1)
 {
 can_msg_received = 0;
 sprintf(msg_send,'CAN Message Received: %X %X\r\n',RxData[0],RxData[1]);
 HAL_UART_Transmit(&huart2, (uint8_t*)msg_send, strlen(msg_send), 0xFFFF);
 }
 }
 return(0);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

stm32l4xx_hal_msp.c

(...)
void HAL_CAN_MspInit(CAN_HandleTypeDef* hcan)
{
 GPIO_InitTypeDef GPIO_InitStruct;
 if(hcan->Instance==CAN1)
 {
 /* USER CODE BEGIN CAN1_MspInit 0 */
 /* USER CODE END CAN1_MspInit 0 */
 /* Peripheral clock enable */
 __HAL_RCC_CAN1_CLK_ENABLE();
 
 /**CAN1 GPIO Configuration 
 PA11 ------> CAN1_RX
 PA12 ------> CAN1_TX 
 */
 GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF9_CAN1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 /* CAN1 interrupt Init */
 HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 1, 0);
 HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn);
 HAL_NVIC_SetPriority(CAN1_RX1_IRQn, 1, 0);
 HAL_NVIC_EnableIRQ(CAN1_RX1_IRQn);
 /* USER CODE BEGIN CAN1_MspInit 1 */
 /* USER CODE END CAN1_MspInit 1 */
 }
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
(...)�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

Thank you for you help.

Miguel

#can #can-bus
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
T J
Lead
Posted on June 26, 2018 at 15:35

this is how I transmit.

 if ((CAN->TSR & CAN_TSR_TME0) == CAN_TSR_TME0)                                                         // (1)

{

 CAN->sTxMailBox[0].TDTR = canTxMsgLength[canTxMsgOUT];                               // (2) length

 CAN->sTxMailBox[0].TDLR = canTxMsgBottomWord[canTxMsgOUT];                     // (3) 4bytes

 CAN->sTxMailBox[0].TDHR = canTxMsgTopWord[canTxMsgOUT];                          // (3) 4bytes

 CAN->sTxMailBox[0].TIR  = ((uint32_t)canTxMsgID[canTxMsgOUT] << 21 | CAN_TI0R_TXRQ); // (4) send it now if the line is idle
Posted on June 26, 2018 at 16:43

Thank you! I'll give it a look! But the mailboxes seem to be full even before I send any message.

Also, I'm using the newer CAN API and I'd like to know what is wrong with my code.

Thank you anyway!