Skip to main content
Gaurav Singh
Visitor II
June 8, 2018
Question

Independent watchdog timer (STM32H743)

  • June 8, 2018
  • 1 reply
  • 787 views
Posted on June 08, 2018 at 15:19

Hello.,.,

I am using IWDG in our application, It is configured for 1SEC timeout . In this I have a requirement to know the Watchdog RESET status, As per reference manual I have seen the register RCC_RSR (bit 26th) but it was not updating even after Watchdog RESET occur. Is there any specific method to read this register or any other way to know the IWDG RESET status.

Any helps would be appreciated lot.,

Regards

GS

#watchdog #stm32h7
This topic has been closed for replies.

1 reply

ST Technical Moderator
June 26, 2018
Posted on June 26, 2018 at 19:07

Hello

gsolankey

,

Are you sure that a reset happened?

May be you should check if the reset pin is toggled.

With Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
June 26, 2018
Posted on June 26, 2018 at 19:18

More specifically, make sure you aren't driving NRST high externally with any of your attached circuitry, this is known to cause failure in many ARM designs.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..