STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Nucleo-303RE Not Starting Up

I am using a Nuclro-303RE to develop a USB Virtual Com port, and I am running into an issue that I cannot seem to resolve.  Just to verify things, I did put some really simple code in the flash the green indicator on the Nucleo board.I have it connec...

Nucleo-F303RE-Clock.png Nucleo-F303RE-USB.png Nucleo-F303RE-VCOM.png Bryon08_0-1744207627697.png
Bryon08 by Associate II
  • 2942 Views
  • 5 replies
  • 2 kudos

Using STMCubeIDE and Micropython

I want to add a USB thumb drive (mass storage) to a NUCLEO-144 F767ZI board. I see the STM32CubeIDE can be used to point GPIO lines PA8~PA12, PG6, PG7 to connector CN13 (USB Micro-AB) or to the Morpho connectors to realize a USB OTG (On the Go) inter...

Resolved! STM32F746ZG DFU MODE

HELLO guys could you please tell me how to put the stm32f746zg board in dfu mode actually earlier i was able to program and use the stlink to dump but currenty im not able to connect using stlink so i want to do with the dfu stm32 bootloader mode i h...

joyson by Associate
  • 2155 Views
  • 3 replies
  • 1 kudos

Corrupted data waveform in specific LTDC data lines

I am going to set up a RGB666 LCD with STN32F779 and Frame buffer in SDRAM. The problem I'm facing is that there are a series of parallel dark lines in the image.I first tested the SDRAM and the reading and writing is done correctly. Then I realized ...

Slh_4-1743094968002.png Slh_1-1743094374198.png Slh_2-1743094447545.png Slh_3-1743094558893.png
Slh by Senior
  • 1263 Views
  • 3 replies
  • 2 kudos

Resolved! Standby mode on stmL433 drawing too much current

Hi   I have a a stm32L433 48 pin processor and trying to get it into low power. I am using the STLink-V3PWR module with stm32Cube Monitor Power module.   First of all I placed a known value resistor across the STLink-V3PWR to make sure it is reading ...

SSmit13_0-1744301600985.png

STM32C0 - use internal oscillators

Hi all,i have selected the MCU STM32C051G8GU6 as the main controller of the RFID system and i am trying to use the MCU without using any external crystals or oscillators, can anyone please guide me how to use the internal oscillators.Thanks in advanc...