STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I program to flash memory through Boundary-Scan JTAG?

I entegrated state machine of JTAG TAP in a mcu for control stm32f103c8t6. It is working well. (IDCODE registers are 0x3ba00477 = CORTEXM3 , 0x16410041 = STM32f103c8 medium lqfp48)But I haven't found any file for programming flash memory with JTAG...

HHuse by Associate II
  • 2063 Views
  • 5 replies
  • 0 kudos

Resolved! Where can I find informations about FIT on STM32 H7 series ?

Hello,I read the numerous document on STM32H7 series especially the safety manual but there is no information on FIT. Some paragraph talk about FMEDA snapshot but I can't find any document.​Do you have technical note about FIT during application ?Tha...

thomas_t by Associate
  • 1401 Views
  • 2 replies
  • 0 kudos

Resolved! Data gets not written in SFR on STM32F429ZIT6

Hey Guys,I hope someone can help me:I testet my software with a STM32F429IDISCOVERY board which works fine. I now designed a custom board and migrated the software. Same peripherals, same pins etc. For a reason I don't understand the ADCs seem not to...

Can I use the SAI block to trigger ADC on STM32H7?

I am using the STM32H743 on STM32H743I-EVAL board.Is it possible to synchronize ADC acquisitions with the SAI block? The goal here is to acquire audio ADC samples using DMA, block process, and transmit out to a DAC over SAI using DMA. The STM32 is th...

markm by Associate II
  • 1844 Views
  • 3 replies
  • 0 kudos

Is there any restricts on SPI feature on Necleo L053R8?

I set the SPI on L053R8 works in slave mode. When the master's clock less than 800KHz, slaver can read/write data success. But when I change the master's clock to 1.6MHz, the L053R8 cannot read one byte any more which is correct, each byte is '0xFF'....

SLiu.10 by Associate
  • 1014 Views
  • 2 replies
  • 0 kudos

SPI problem with STM32L496 and package 1.13.0

Hello,after updating STM32Cube​MX 4.27.0 with package 1.13.0 for STM32L4 I have a problem with SPI communication. I've replaced the file stm32l4xx_hal_spi.c with the old from 1.12.0 and it works.Can you check if there is any bug in stm32l4xx_hal_spi....

SStor by Senior
  • 1362 Views
  • 5 replies
  • 0 kudos