Dear sir,I am using STM32F769NI microcontroller. I want to glow to different Leds on one external interrupt line i.e. Led1 on rising edge and Led2 on falling edge. Can you please suggest me the solution.Regards,Manoj
I am using STM32L010K4. I want to reduce the sleep current to 3uA ,But in the datasheet it is mentioned the the minimum sleep current is 1mA with all the peripherals disabled, which is a larg value
Ok. But in my case the level 0 appears in two cases first when logic 0 is applied and second when the line is disconnected. So what shall I do in this situation?
My high voltage will not be more than 400VI want the exact value is there any need to compute it.What do you mean by that, because we already have it inside the chip isn't ? do we also have option to enable/disable it ? In which case should we opt f...