Mark and Space parity on UART?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-11-06 3:26 PM
Does anyone know if you can set Mark or Space parity on the STM32 USARTS?
I only found that you can set Even or Odd parity so far. I need to configure an STM32 for hardware that uses Mark and Space parity bits so any help would be appreciated. Thanks,Devyn #uart-mark-space-parity- Labels:
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-11-06 3:59 PM
Does anyone know if you can set Mark or Space parity on the STM32 USARTS? I only found that you can set Even or Odd parity so far. I need to configure an STM32 for hardware that uses Mark and Space parity bits so any help would be appreciated.
Set it to 9-bit mode, no parity, and send whatever data patterns you want.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-11-07 12:15 PM
Thanks for replying, Clive, but how would I send a 9 bit character through the UART? Maybe I'm missing something that's really easy, but I can't think of it.
What I need is to send a message like this:Hex, Binary, Decimal equivalents:
0x115 0b100010101 277 (this is really 21 with a mark parity set)
0x002 0b000000010 2
0x000 0b000000000 0
0x03b 0b000111011 59
0x000 0b000000000 0
0x000 0b000000000 0
0x000 0b000000000 0
0x052 0b001010010 82
so you see, first byte has mark parity(MSB) while all others are space. Just before sending the first byte, I tried to set the UART to 8N2 which should be the equivalent of a mark parity, then set it back to 9N1 before sending the rest of the bytes, but it doesn't seem to change anything. It still sends without making the MSB a 1 for the first byte. Here is my code:uint8_t Message[0] = 21;
uint8_t Message[1] = 2;
uint8_t Message[2] = 0;
uint8_t Message[3] = 59;
uint8_t Message[4] = 0;
uint8_t Message[5] = 0;
uint8_t Message[6] = 0;
uint8_t Message[7] = 82
//set USART3 to 8N2 before sending first byte
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_2;
USART_Init(USART3, &USART_InitStructure);
//send first byte
while(USART_GetFlagStatus(USART3, USART_FLAG_TXE) ==RESET);
USART_SendData(USART3, Message[0]);
//set USART3 back to 9N1
USART_InitStructure.USART_WordLength = USART_WordLength_9b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_Init(USART3, &USART_InitStructure);
for (i = 1; i < 8;i++)
{
while(USART_GetFlagStatus(USART3, USART_FLAG_TXE) == RESET);
USART_SendData(USART3, From_MATE_Message[i]);
}
Thanks,
Devyn
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-11-07 12:29 PM
You'd want to wait on TC before shifting gears.
Or frankly just use 9N1 with USART_SendData(USART1, 0x100 | FirstByte); and USART_SendData(USART1, SubsequentBytes & 0xFF);Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-11-07 12:43 PM
Clive,
Just tried what you said. Works great! Thank you so much for your help! I thought that I had actually tried that before, but here's what I did wrong:Message[0] |= 0x100;
USART_SendData(USART3, Message[0]);
I tried ORing then setting it back into the 8 bit character which didn't do anything, because it only allows 8 bits, but if you do the calculation in the function it will send that 9th bit along with the 8 bit character.
Anyways, thanks Clive! Was working on this issue for a while trying to figure it out.
Devyn
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-08-21 7:40 AM
With STM32CubeMX, under UART configuration. Why is there no mark parity option available.
Has there been any other workarounds other than above. Above method works though, but is rather troublesome.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-08-21 8:06 AM
> Has there been any other workarounds other than above.
Using an external UART.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-08-21 10:14 AM
>>Why is there no mark parity option available.
Because the hardware doesn't commit gates to implementing niche functionality.
Use the 9-bit mode and send/receive/check whatever patterns you want.
Why is this troublesome/complex? You're not having to implement a soft-uart.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-08-21 12:29 PM
... as if soft-UART would be troublesome or complex... ;)
JW