User Activity

Hi. I think I have an idea why this does what it does, but wanted to ask advice anyway.I am interfacing an STM32F767 over SPI with an SSD2828 parallel RGB to MIPI bridge.It (amongst other options), uses what they describe as 24 bit SPI.I am using the...
With the recent acquisition, is TouchGFX going to become free to stm32 users? If so when? Soon? 8)
Posted on July 15, 2018 at 02:10Hi.I am doing well. The Panasys 3.4' round TFT (actually it's about 2.4' round, in an octagon, that was probably cut from a 3.4' square once upon a time) MIPI DSI display is working on the stm32l4r9i-discovery, after ...
Posted on July 13, 2018 at 00:50Hi. I am trying to compile the STemWin Demo code for L4R9I-DISCO in TrueStudio and failing miserably.Firstly I did the import procedure which is supposed to make it easy to get all the Cube demo stuff into True Studio...
Kudos from