cancel
Showing results for 
Search instead for 
Did you mean: 

Why such an insane value for SDMMC_CMDTIMEOUT?

Why is the value for stm32f7xx_ll_sdmmc.h's SDMMC_CMDTIMEOUT (5 seconds!) so insanely huge as compared to the Reference Manual SDMMC_STA.CTIMEOUT description and the MMC Ncr timing?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

You think that's a long time...

#define SDMMC_DATATIMEOUT                 ((uint32_t)0xFFFFFFFFU)

#define SDMMC_CMDTIMEOUT                  ((uint32_t)5000U)       /* Command send and response timeout */

#define SDMMC_MAXERASETIMEOUT             ((uint32_t)63000U)      /* Max erase Timeout 63 s           */

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Yeah, I've seen those too. It'd be helpful if there was some commentary explaining such ludicrous values, especially in the case of SDMMC_CMDTIMEOUT, which should rightfully have a value no larger than (64 + 48 + some_small_number) * (SDMMC_CK period).

Hello, ST? 5 seconds checking for bits that should (must!) be set in << 1 mSec?