cancel
Showing results for 
Search instead for 
Did you mean: 

Want know about this error in the picture..?

Ahami.4
Associate

Hello,

I am using STM32F070*B Nucleo board want to flash the device using Flash Loder demonstration software using UART communication. but this type of warning message came.

Link that i am following:

http://stm32f4-discovery.net/2014/09/program-stm32f4-with-uart/

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Indicating the device is not in loader mode. Make sure BOOT0 is high and reset, entry is a one shot deal. Make sure UART being used is supported by loader. Use 9600 with EVEN parity. ​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Ahami.4
Associate

hii Clive,

Boot 0 pin is high and device on the loader mode. UART is also supported by the loader,9600,even parity,protection level also checked. i am use the correct pin out. any other reason for this error..?

entry is one shot deal..? you mean delay..?