User Activity

Hello!I bought a new STM32F469 discovery kit and wanted to test it. since there was no initial program installed (checked by connecting with the USB port) I tried to launch one of the demonstrations from the firmware package over STMCubeIDE (Vers. 1....
Hello!I wanted to check the TouchGFX demonstration for the STM32F746G-DISCO and imported the project via STMCubeIDE (1.10.1). The project builded without errors and can be debugged. Sadly I get the following Screens. Does anybody know why this demosn...
The project is in the e-mobility sector (pedelecs, e-bikes)the MCU needs to be compliant with SAFERTOS and SIL levelselectric engine and electric generator signal regulationCAN bus compatibledisplay compatible (LCD or TFT)ADC/DAC featuresbluetooth an...
Hello,I have come over this bug per coincidence:I am doing an evaluation project with the STM32F407G-DISC1 Board and want to utilize the DMA together with the I2S to feed the Audio data to the CS43L22 DAC.Since interrupt driven I2S transmit HAL funct...
Hello,I am trying to get FreeRTOS and SEGGER SystemView (3.1) to run on an STM32F103RCTx. I used the appropriate manual from SEGGER to include all the necessary folders in my project. Although I have included all the new folders in the Include Paths ...
Kudos from