cancel
Showing results for 
Search instead for 
Did you mean: 

Data gets not written in SFR on STM32F429ZIT6

Benjamin Brammer
Senior II

Hey Guys,

I hope someone can help me:

I testet my software with a STM32F429IDISCOVERY board which works fine. I now designed a custom board and migrated the software. Same peripherals, same pins etc. For a reason I don't understand the ADCs seem not to work. I want to use ADC3 and ADC1 and have already tested and used them correctly with the DISCOVERY board. What I find quite strange is that I only see zeros in the ADC SFR view. As if the peripheral is not being set up allthough the routines are executed when I step through them with the debugger The DAC -which I also use - seems to work except for a 3mV error which is tolerable I think.

I set up everything with STM32CubeMX and debug with true studio. All latest versions including the latest HAL and firmware package.

Does anybody know what is wrong here?

best regards

Benjamin

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

Is the ADC clock enabled in RCC?

JW

View solution in original post

5 REPLIES 5
waclawek.jan
Super User

Is the ADC clock enabled in RCC?

JW

Benjamin Brammer
Senior II

Hey Jan,

thanks for your fast reply!

Yes you are right! The ADC3EN bit in the RCC_APB2ENR is not set. But I truely don't understand this. I did the same initialization routine and settings I have with the former DISCOVERY board... except that I have two different CubeMX project files. One with the DISCOVERY board and one default with only the processor. Do you know where I can set this in CubeMX? I thught this was done automatically as I activated the pripheral in the analog tab.

Benjamin

Benjamin Brammer
Senior II

Well there is one difference from my RCC clock source: the DISCOVERY board uses a ceramic crystal and I use an oscilator. so I set HSE to BYPASS Clock source. Could this be a problem?

Benjamin Brammer
Senior II

Ok..I think there is some problem inside my routines...I don't get it at the moment. But the ADC3 Clock is enabled in the HAL routines and it gets enabled, but is later disabled as I start TIM7 as a free running timer...I will have to look deeper into this.

But thanks for your fast answer and the help! :)

found the problem: I have an EXTI that gets triggered which deactivates the peripheral. I know why this is. So basically the hardware and software does what it should. It's just me being the problem :D