STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VGA not working?

I am trying to give 800x600@56hz vga output with my stm32f103c8t6. For some reason I can't get it to work. Both of the monitors I tried are saying "Input is not supported" or sth along thoose lines.I know that they can work with 800x600@56hz. I have ...

FEkic by Associate II
  • 1592 Views
  • 2 replies
  • 0 kudos

Resolved! Memory Mapped QSPI reads nonsensical data

I am using a STM32F746zg uc connected to a W25Q80 Flash memory. In my initialization I erase a page then memory map the flash and then I read a pointer to that address. I expect to read 0xFF as the flash has just been erased, however I read 0x88. I'm...

Resolved! STM32F429 video output protocol for a SVGA display

Hello,I'm looking to use the STM32F429 to output data to an SVGA display. The supported video formats for the display are shown in the image below. The display is actually a monochrome variant, so color is not relevant as the RGB lines are tied tog...

0690X000009ZhkeQAC.jpg
MRyan.7 by Associate III
  • 1307 Views
  • 1 replies
  • 0 kudos

QSPI error at border 0x01000000

Chip stm32f746, memory S25FL256S in 32-bit address mode.An error occurred while sharing DMA and reading directly on the edge of the address 0x01000000.The error occurs when the high fourth byte of the memory address is changed. When DMA and reading o...

SDRAM and adc warnings

I am evaluating the STM32F767NIH. I am finding the warnings a bit unclear for the FMC. A brand new project with only the fmc shows a warning triangle that I can't seem to get rid of. I have checked Clock and chip enable SDCKE0+SDNE0, 2 banks, 13 bi...

_EFrie by Senior
  • 851 Views
  • 0 replies
  • 0 kudos