STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 - USB HS Host - nothing happens

Hi there,​I got some troubles getting the USB Host system working on the STM32H746ZI.​Worth mentioning is that this is no dev board here, just a plain H7 mcu on a DIY bread board. It is properly supplied with filtered 3.3 and 1.8V. Got UART, I2C, LCD...

Microman by Associate III
  • 8047 Views
  • 10 replies
  • 1 kudos

what's the problem?

hello everyone,can someone help me please, I can't understand why I can't receive 7, it's weird... I sent 7 , i want to receive 7, but I receive 255, 0, 15.. all the values except 7, that's really insane.

0690X000009ZeWtQAK.png
idrissmc by Associate III
  • 6355 Views
  • 20 replies
  • 0 kudos

CAN_ESR LEC[2:0] Error meanings

These are the CAN error codes listed in RM0008 (Manual for STM32F1)Is there anywhere in documentation that says what they actually mean in detail? Are these detected on RX or TX. I assume that in this case its TX and, while active an error frame will...

DJC by Senior
  • 2554 Views
  • 2 replies
  • 0 kudos

Resolved! Unique ID seems to be there, but the documentations says no

I need a unique ID and expected to use the 96 bit one from the chip. Then I read that STM32F070x6/B do not have it. Very disappointing, but I looked at the F0 location 0x1ffff7ac and sure enough there is something that looks exactly like a described ...

AFree by Associate
  • 1254 Views
  • 1 replies
  • 0 kudos

Level triggered interrupts on STM32L series

I'm working with the STM32L152. I have a USB port which has a detect signal connected to an IO pin. When the USB plug is inserted or removed the detect pin changes state. On some occasions the signal is missed. Looking at the signal on the scope sho...

LThal by Associate III
  • 2414 Views
  • 2 replies
  • 0 kudos

Moving from STM32L476xx to STM32L4R9xx

After spending some time looking into the R9 I decided to make the switch. I've been developing on the 76 for a while now. I read the migration document and it doesn't look like there are any differences.​Right now I'm having issues with spi and sd c...