STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Loading FW to STM32 IoT Discovery Kit

Hi there,I got stuck at the most basic step but couldn't find a step-by-step guide to get through it. Any pointer to a guide for me to follow is appreciated.I am trying to download a built FW to my STM32 IoT Discovery kit. However, when i connect m...

CLiu.0 by Associate
  • 5176 Views
  • 1 replies
  • 0 kudos

afe4300 and stm32f103rb, rdy pin unchanged

Posted on May 23, 2017 at 12:04Hello,I have a problem in getting the ti AFE4300 start the ADC measurement. I started with a new board that was designed using reference design on TI. Am trying to communicate with the board through an stm32f103rb(nucl...

I try to use hard ecc of stm32f767igt under U-Boot,but i test my code ,i found could only write one page by one page under command of U-Boot,

I try to use hard ecc of stm32f767igt under U-Boot,but i test my code ,i found could only write one page by one page under command of U-Boot,then i will get the right ecc value when i ready after i will one page ;but when i write two page or more, i ...

SmartCard example for STM32H7

HI, I am trying to implement smart card reader on this chip. I got the ATR from the card, and tried to port AN4800_FW_V1.0.0 examples but without success. Do you know when some example for this chip will be avaliable?

larenge by Associate II
  • 3539 Views
  • 8 replies
  • 2 kudos

Resolved! USART bare metal programming fail to send data - STM32L4R5ZI

I am new to embedded programming and trying to learn ARM with my STM32L4 board. I stick to the datasheet and stay away from HAL library to learn how the MCU and its peripherals work. Here I am trying to initiate USART3 and send a line using "printf" ...

KHuyn by Associate II
  • 5394 Views
  • 11 replies
  • 0 kudos

Resolved! Calling a function by it's address not working

Using a STM32F0 discovery board, I have this function:void BlinkBlue(void) { for (int i=0; i<20; i++) { HAL_GPIO_WritePin(LD4_GPIO_Port, LD4_Pin, GPIO_PIN_SET); HAL_Delay(50); HAL_GPIO_WritePin(LD4_GPIO_Port, LD4_Pin, GPIO_PIN_RESET); H...

NNar by Associate II
  • 1705 Views
  • 2 replies
  • 0 kudos

How do I use a timer to wake up from sleep on the STM32F405RG

I hope I posted in the right spot. I'm using a STM32F405RG cpu. I can't figure out how to sleep and wake up using the timer. The code I found online uses 'pwr_enter_standby_mode()' which may affect the reason why I can't wakeup. I see in RTClock.h th...

AOIjd by Associate
  • 797 Views
  • 0 replies
  • 0 kudos

STM32L0 ADC+TIM

//Enable ADC1 begin =========================================================================================================================================== RCC->APB2ENR |= RCC_APB2ENR_ADC1EN; __NOP();   ADC1->CR = 0; //off ADC   //ADC interru...

Jumping to Application inside main not working

Hi, I am using STM32f429 I am trying to do FOTA. After the bin file is flashed when I tried to jump from main using jump to run the code which uploaded at the other address not working the code get stuck into the hard fault handler can anyone help me...

AChan.15 by Associate II
  • 1149 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.