STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART receive interrupt

I'm trying to take input from user via serial port. I use STM32's USART1_IRQHandler and sscanf functions. Although I can print message on the port by using sprintf, I can't take input with sscanf. It doesn't wait for input and assigns a value I can't...

DAyva by Associate
  • 1653 Views
  • 3 replies
  • 0 kudos

STM32H7 Series lifetime estimates

An interesting appnote has appeared, AN5337 STM32H7 Series lifetime estimates.It's not that usual to be concerned about the lifetime of a mcu. Megahertzs take their toll.JW

In LP RUN mode can I use SAI2

I'm using an STM32L476 as an analogue to digital streaming device. Analogue -> ADC -> DMA ->SAI -> External Device. The SAI runs as a Time Division Mutiplexed (TDM) slave, with the data clock and frame sync are received from an external device. The d...

RLamk.15 by Associate
  • 705 Views
  • 0 replies
  • 0 kudos

nitially when the microcontroller is started up it should start with some default PWM with some fixed duty cycle(say 65%), but i want it to start slowly (soft start ) rising (LIKE A RAMP) need HElP/Support in adding this feature

 I have developed a PID control loop where PWM has to adjust itself to give the desired outputand the PWM is controlled by ADC and reference voltage.initially when the microcontroller is started up it should start with some default PWM with some fixe...

GH M by Associate II
  • 1521 Views
  • 1 replies
  • 0 kudos

Count external pulses on timer 3 channel 4 STM32F415

Hi, I am currently facing the problem, that we made a new product and slightly changed the design and routing from the old version and now the input for counting pulses in on PB1. I would like to count pulses on tim3 channel 4 and I am really not sur...

capture by Associate
  • 1349 Views
  • 1 replies
  • 0 kudos

how to use EXTI in stm32F030?

There are 3 interrupt handler EXTI0__1 ,EXTI2__3, EXTI 14__5how they can be used since it can be working in EV board but i am not able to work it in STM32F3K6