STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L073CZ

Hi, I'm using the STM32L073CZ micro in a thermometer application.I've used CubeMX to create the base code and adapted it.I'm using ADC channel 1 for the temperature measurement, which is working correctly. I'm only initializing the ADC channel when i...

couldn't able to get the can bus working!!!

Hi,I have two projects. one project i have generated using cubeMX and another one i have imported from example project of STM32F769I_EVAL .I'm using Nucleo-f767zi board.I have configured both the projects in the same way but the STM32F769I_EVAL proj...

VPras by Associate II
  • 786 Views
  • 0 replies
  • 0 kudos

Setting the USART baud-rate

Hi Everyone,We have managed to increase the clock speed for STM32F722 using PLL. Now we are wondering how we can keep the baud rate of USART6 to 115200 bit/s (is there any function/capability in STM32F722 that automatically adjusts the USART clock di...

DHes by Associate II
  • 8364 Views
  • 10 replies
  • 1 kudos

UART receive interrupt

I'm trying to take input from user via serial port. I use STM32's USART1_IRQHandler and sscanf functions. Although I can print message on the port by using sprintf, I can't take input with sscanf. It doesn't wait for input and assigns a value I can't...

DAyva by Associate
  • 1737 Views
  • 3 replies
  • 0 kudos

STM32H7 Series lifetime estimates

An interesting appnote has appeared, AN5337 STM32H7 Series lifetime estimates.It's not that usual to be concerned about the lifetime of a mcu. Megahertzs take their toll.JW

In LP RUN mode can I use SAI2

I'm using an STM32L476 as an analogue to digital streaming device. Analogue -> ADC -> DMA ->SAI -> External Device. The SAI runs as a Time Division Mutiplexed (TDM) slave, with the data clock and frame sync are received from an external device. The d...

RLamk.15 by Associate
  • 743 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.