STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C_frequency configuration

Hi,I would like to configure the I2C frequency based on the input clock frequency. Is there a specific formula to calculate the I2C timing values? Also, I would like to know whether this formula is applicable to all STM32 microcontrollers, or if it v...

SDhar.1 by Associate II
  • 1171 Views
  • 2 replies
  • 2 kudos

Issues with interrupt priority handling

Hello,i have configured a timer interrupt an it seems like that interrupt preempt another adc interrupt. I configured the timer interrupt like that: NVIC_SetPriority(TIM1_BRK_IRQn, 2U); NVIC_SetPriority(TIM1_UP_IRQn, 2U); and the adc interrupt like t...

Resolved! STM32L011 bootloader cannot read SRAM

I have an STM32L011 on a board I am developing.I can enter the bootloader no problem, as per AN2606/AN3155.  I am using USART2, 57600 baud.I can program FLASH/erase FLASH/read FLASH - all works as expected.I note that the bootloader reserves 2048byte...

Resolved! Project not picking up RAM section from linker file

I am working with a dual core STM32H755 and attempting to create a shared memory location for the two cores to access. I am attempting to do this by modifying the linker script.  I have added the following lines to the M7 core linker script, in the S...

TomC1_0-1746627364480.png
TomC1 by Associate III
  • 2250 Views
  • 5 replies
  • 1 kudos

硬件不变的情况下,SPI+DMA 循环模式主机接收 采集电压异常,Normal模式却正常

用SPI+DMA驱动AD4001,用片选信号代替 CONV,采集一个正弦信号。Normalnormal正常,循环模式却不对,求大佬解答!!Normal模式下,每次在 HAL_SPI_RxCpltCallback 函数里面重新启动数据正常,能看到正弦变化规律                                 循环模式下数据就不对了,采集的同样一个交流信号,我在半传输完成回调里面查看,按道理后半部分的数据应该是正常的正弦变化才对,实际却不是,但是去采集直流时又是正常的。        ...

154804hzpook13om0ogbkz.png 154808z1jn00040jl06znf.png 154810og0gd6z72v30cgzv.png
kevin_sa by Associate
  • 1045 Views
  • 1 replies
  • 0 kudos

STM32H5 GPDMA Linked list example without HAL

I am trying to implement a GPDMA driver in a C project that does not use HAL, and have been really struggling to get something working. I have read everything I can find on this peripheral, multiple times, and still don't quite understand how one wou...

tbennett_0-1746647568608.png
tbennett by Associate
  • 1345 Views
  • 1 replies
  • 0 kudos