User Activity

Hi there,I have a custom board with an STM32F070. The VDD and VDDA are connected together. System runs at 48 MHz from a 8 MHz crystal. Each VDD has a 100nF cap. VDD is 3.3V, from a 1% LDO.The code uses UART1, UART2, USB and I2C2. Also, many I/O pins....
Hi there,I have a custom board (with eMMC) that freezes in the middle of kernel loading:I am under the impression it is related with the rootfs.ext4, becuase it does not try the loading, but I am not sure yet.Flash table is the following (I don´t use...
Hi ST Community,I am trying to flash a eMMC with STM32CubeProgrammer, in a STM32MP157F custom board. I am using a GPT partition file and a img.I can see the system is creating partitions and flashing, but the structure is wrong for eMMC, so it does n...
Hi there,I have a custom board based on STM32MP157F, with USB2 connected to STM32CubeProgrammer for flashing the eMMC. No USB-ID, no USB-VBUS connected.The STM32CubeProgrammer downloads the FSBL and U-Boot, but the software does not reconnect as "USB...