User Activity

Hi,What are the different power saving mode for STM32H753 with there current consumption. What are the active functions in each mode?
We are planning to use STM32H753X in one of our design. For JTAG interface I can see two options 5 pin and 4 pin JTAG. Is STM32H753 supports 4 pin JTAG? If yes, how to manage NJTRST pin? Shall i connected NJTRST pin to NJRST?  what is the use of 5 pi...
Hi, Can we use any UART /USART port for debugging? or any dedicated port only i have to allocate for debugging purpose? what are the main application where USART can be used and UART cannot be used?
Hi,I am using STM32H753XI in my ongoing design. We are using most of the timers and internal ADCs in our application. So it is very tough for me accommodate both external eMMC and NOR flash interface.  My question is, Can we boot STM32H753 with exter...
Kudos given to