STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

General availability?

The device was announced over a year ago. Any news on a date for its move from evaluation to production?​

Hedley by Associate III
  • 1627 Views
  • 4 replies
  • 1 kudos

STM32F429 and pcm1808 some I2s question

Hello. Please help me.I want to use pcm1808 ADC in 24bit mode. pcm1808 have a two channels, left and right. I'm generate some code in CubeMX and send recv data to pcm5102 DAC. The sound is transmitted to both channels. But I need to take only the lef...

Igor1 by Associate
  • 2827 Views
  • 2 replies
  • 0 kudos

SD lossless data storing from GPIO.

Hello,I am thinking to use an STM32H7 to write external data incoming from 16 GPIOs to an SD using the internal SD 4.1 Host controller. The data clock rate is 12 MHz.The STM32H742xI/G STM32H743xI/G DS (https://www.st.com/resource/en/datasheet/stm32h7...

simo zz by Senior II
  • 2138 Views
  • 5 replies
  • 0 kudos

STM32F373 SDADC HAL after Calibration, do I need to manual put an offset error value to final calculate with sdadc output value?

HiAs a title, after I call HAL_SDADC_CalibrationStartand HAL_SDADC_PollForCalibEventfollow Refference Manual page 240, calibration progress will store an offset error value in OFFSETx[11:0] fields. So do I need to read this value and put in the calc...

NNam.18 by Associate II
  • 984 Views
  • 0 replies
  • 0 kudos

STM32072B-EVAL Display

Hi, Just purchased a STM32072B-EVAL board and loaded an example project on it. I cleared it from memory using ST visual programmer and now the LCD display is blank (i use to see the GUI). Did i accidentally erase the GUI? If so can I download it back...

canucktut by Associate II
  • 1402 Views
  • 3 replies
  • 0 kudos

STM32F100 RTC Wake From Standby is always 1 Second Late

Hello,I use STM32F100RBT. I want to enter STANDBY mode and exit every second.It works well, except for one issue: it always wakes up 1 second later.I run the following code, where I get the current time, print it and set an alarm for the next second ...

ISeed by Senior
  • 1713 Views
  • 1 replies
  • 0 kudos