Skip to main content
Pa.6
Visitor II
June 1, 2019
Question

STM32 Beginner: needs help on ADC with STM32F103r8

  • June 1, 2019
  • 1 reply
  • 747 views

Hi,

I am a beginner for stm32. I am using stm32f103r8 , IAR-ARM IDE.

I have attached my celow , this is not working , i am checking it in Proteus 8.8v ( with stm32f103r6). Can anyone help me out with this ?

PROGRAM:

#include "stm32f10x.h"

#include "stm32f10x_adc.h"

void main()

 {

   RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); //Enable ADC1..//

   RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);

   RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE); //Enable Port C..//

    GPIO_InitTypeDef GPIO_InitStruct;

    GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AIN;

    GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0;

    GPIO_Init(GPIOB, &GPIO_InitStruct);

    GPIO_InitStruct.GPIO_Mode = GPIO_Mode_Out_PP;

    GPIO_InitStruct.GPIO_Pin = GPIO_Pin_1;

    GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;;

    GPIO_Init(GPIOC, &GPIO_InitStruct);

    //----------------------------ADC Initialize------------------------------//

     ADC_InitTypeDef ADC_InitStructure;

     ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;

     ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

     ADC_InitStructure.ADC_ExternalTrigConv = DISABLE;

     ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;

     ADC_InitStructure.ADC_NbrOfChannel = 1;

     ADC_InitStructure.ADC_ScanConvMode = DISABLE;

     ADC_Init(ADC1, &ADC_InitStructure);

     ADC_Cmd(ADC1, ENABLE);

     //----------------------Selecting input Channel--------------------------//

     ADC_RegularChannelConfig(ADC1, ADC_Channel_9, 1, ADC_SampleTime_1Cycles5);

     //-------------------------Start Conversion------------------------------//

   for(;;)

   {

     ADC_SoftwareStartConvCmd(ADC1, ENABLE);

     while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC));

     ADC = ADC_GetConversionValue(ADC1);

     if(ADC > 500)

     {

      GPIOC->BSRR = 0X0000000F;

     }

    else

    {

      GPIOC->BRR = 0X0000000F;

    }

 }

 }

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
June 1, 2019

When using as local/auto variables I'd recommend clearing them properly

GPIO_InitTypeDef GPIO_InitStruct ={0};

ADC_InitTypeDef ADC_InitStructure = {0};

>>this is not working

Yeah that's not very enlightening, use the debug step the code, review the settings in side the peripherals, try to understand the mechanics of the failure.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..