STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Write and Read from SRAM on STM32H7

Hi, I'm trying to do a read and write to an FMC, SRAM Bank 1, NE1. However, it does not work.STM32CubeMX was used to create the setup.The SRAM setup:static void MX_FMC_Init(void) {   FMC_NORSRAM_TimingTypeDef Timing = {0};   /** Perform the SRAM1...

Kcube by Associate
  • 1652 Views
  • 0 replies
  • 0 kudos

STM32L051 won't restart with LSE soldered even if using LSI

I have multiple boards with a STM32L051 MCU and 2 board revision, A and B.A: no LSE oscillator, LED connected via 550 Ohm resistor, around 20uF capacitance on VCC, radio module solderedB: 6pF 32kHz +-20 ppm oscillator soldered, 9pF load capacitors, a...

ramses946 by Associate III
  • 1510 Views
  • 2 replies
  • 0 kudos

SPI dma example receiving only 0

Hi I am using stmh7 nucleo board and trying the spi dma example in NUCLEO-H743ZI folder, but thr transfer only gives me 0 in the aRxBuffer, anyone has had this problem before? I am not sure how to solve thisThanks!

The speed of the stm32 GPIO (different series).

Dear engineers. I want to read an extern parallel ADC directly connected to GPIO ports of stm32 microcontroller and clocked from it. It is necessary to make 1000 readings from the ADC with a maximum speed and write them to stm32 memory. What is the m...

stm32f411 tim5 and tim9 can not use to be TIM_Encoder mode

int main(void){ HAL_Init(); BSP_LED_Init(LED3); BSP_LED_Init(LED4);BSP_LED_Init(LED5);BSP_LED_Init(LED6); /* Initialize TIM3 to emulate a quadrature encoder outputs */ Init_TIM_Emulator(&EmulatorHandle);   UartHandle.Instance     = USARTx;   UartHand...

yuming by Associate II
  • 1605 Views
  • 3 replies
  • 1 kudos

How to stabilize the SDADC2 in STM32F373VCT6?

When I connect a voltage source to channel 0 of SDADC2 in single ended mode, then at floating pin and connecting to ground the value displayed is full scale which 65535, while when I connect some voltage like 2V or 3V to same channel then it shows t...

STM32F4 program crashes when interrupt is activated

Hello,I wrote a program for the STM32F4 using the Standard Peripheral library from ST. I compile the source code with the ARM-GCC tool chain and flash it on the chip using OpenOCD in combination with gdb. As long as I do not use interrupts everything...

NAtta by Associate II
  • 4958 Views
  • 8 replies
  • 0 kudos