STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F769NI Evaluation board NEWBIE

Hi AllI am just starting off with the STM parts and bought the 469 EVM. I got the touch ID with TouchGFX working and made some cool things but now it is time to start using the periphials on the board in bare metal C config.I am really looking to do ...

Can I use the Quad SPI memory controller peripheral on STM32F4xx series to access a PSRAM or SRAM IC rather than a flash IC, and have the data memory map as if internal RAM?

I am hoping to use the CMSIS/DSP libraries to work on data that I periodically store on external RAM. If it is important, my current plan is to use the Lyontek LY68L6400 PSRAM or the VTI7064 SRAM (more expensive). Both are 64Mb volatile memory ICs th...

PDR_ON effects to VBat?

Datasheet says Yes, but as we tested, RTC still runs (hold data after disconnected power), no matter what state of the pin is.Thanks for any suggesstion!

Dat Tran by Senior II
  • 801 Views
  • 1 replies
  • 0 kudos

Interfacing between SMT32F and ST L6206

Previously I've designed a motordriver based on an STM32F303 and an ST L6206 Dual Full Bridge driver. I've had some issues with the interfacing between the MCU and the bridge driver, because the MCU works on 3V3 and the bridge driver works on 5V. So ...

MAkke by Associate III
  • 1594 Views
  • 0 replies
  • 0 kudos