STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with WiFi Connection in board B-L475E-IoT01A2

I have purchased a B-L475E-IoT01A2 board that WiFi connection works well in the company. But the problem is that when I take this board home and test it, it doesn't connect to Wifi. It should be noted that in both cases, I test this board with my mob...

Slh by Senior
  • 743 Views
  • 0 replies
  • 0 kudos

flash using USART for STM32F303E- eval

hi stm,i want to flash using USART. what is procedure.flashloader demonstrator is not working, it is getting hanged (win 7). but target is WIN XP.mcu board is need to connect with WIN-XP PC. how to achieve the target.

How to change output frequency of timer during run time

I am using stm32L073Rz I am using Tim2 channel 3 to generate different frequenciesAs per an example ,i configure timer 2 channel 3 in TIM_OCMODE_TOGGLE modewhen i generate code using cubemx i get the desired frequency using below code snippetbut i wa...

SA.17 by Associate III
  • 3974 Views
  • 4 replies
  • 0 kudos

STM32F030CCT6 pins connection

Hi,I'm very new to this STM32 MPU, I'm trying to setup a tracking device using STM32F030CCT6,GPS module and a sim.Please help me out with the setup and also please let me know the connections as I could not get enough data from the datasheet.Thanks i...

BMC.1631 by Associate
  • 760 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F427 DMA transfer error -- why? (not CCM issue)

Hi,I'm getting a DMA transfer error on an STM32F427, but don't know why. I've already ruled out memory areas (ie. CCM) not accessible by DMA. Here are my registers:As you can see, S0M0AR is located in SRAM, S0PAR is a GPIO BSRR register. The transfer...

0690X00000AsR1iQAF.png
Szabi by Associate
  • 2911 Views
  • 2 replies
  • 0 kudos