User Activity

I have an LIS3DSH securely mounted to a stationary object away from any vibration. Over the course of two and a half days, I've found the readings slowly change in value. I've tried this with multiple accelerometers (all LIS3DSH) and they always sh...
I've used the LIS3DSH state machine to set the INT1 interrupt high when a certain acceleration threshold is exceeded. However, I'd like to use the state machine to detect a change in orientation.For example, I'd like it to set the interrupt high whe...
Hi, I've had an STM32F411 development board for sometime and have done hobby projects with practically every peripheral on the board (audio output, mic, accelerometer, gyroscope, etc) programming both with and without the HAL. I'm now interested in ...
Posted on June 08, 2018 at 17:58Can someone please clarify what the use case for the offset registers are on the LIS3DSH accelerometer?  These are registers OFF_X (0x10), OFF_Y (0x11) and OFF_Z (0x12).  The http://www.st.com/content/ccc/resource/tec...
Posted on May 27, 2018 at 18:12Hi, I'm using an LIS3DSH in a case where I want to periodically (say once every 50 milliseconds) get the most recent X,Y,Z position of the accelerometer and perform a calculation.My current approach is to just set a ti...
Kudos from