STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103RDT6 Pin details

Hi,I am using STM32F103RDT6 for my project. I need only two seperate uart lines and 2 Gpios for to connect 2 RS485 transceivers.I need TX ,RX pin only. So what about the CTS & RTS pin. can I make that as float?There is 2 boot pins in the IC. how I co...

Mom.1 by Associate II
  • 2231 Views
  • 4 replies
  • 0 kudos

CANFD frame format !!!!!

hello ST Community ,the frame format settings of the CANFD are missing FDCAN_FRAME_CLASSIC !!!!I can set this format only with hand in the software but as soon as i try to generate a new code this setup would be overwritten with the available setting...

Moha-Affa by Associate II
  • 1108 Views
  • 0 replies
  • 0 kudos

STM32L151C8T6 USART1 works from time to time

Hello.I'm using STM32L151C8T6 for some simple task. In the beginning I used MSI clock and everything was fine. But I decided to switch to HSI and now I got problems using USART1, namely I think that the USART1 periphery isn't properly initialized due...

kaloyan by Associate III
  • 2212 Views
  • 5 replies
  • 0 kudos

Timer Configuration for specific duration

Hello ,I want to configure a timer which start and runs for specific duration and stops automaticallyand when again i want to start that timer i could be able to start timer and agian stops automaticallyduration is fixed all timeDipak Garasiya

Timer configuration

i want to implement a timer which make a perticular pin to toggle at perticular time duration the duration could I set manaully.

FDCAN Bittiming Problem __ STM32H750 __

Hi,my question is simple , i have these parameter :Can_Clock = 48 MHz Prescaler = 1;NominalTimeSeg1 = 18NominalTimeSeg2 = 4and this is the MX_FDCAN1_Init() :static void MX_FDCAN1_Init(void) {   /* USER CODE BEGIN FDCAN1_Init 0 */   /* USER CODE E...