isar�
Associate II
since
2019-07-05
2023-06-14
User statistics
4
Posts
0
Solutions
0
Kudos given
1
Kudos received
STMicroelectronics Community
About isar�
Options
Report User
User Activity
Posts
Replies
How to get 4 channel input capture values from stm32f407 ?
2019-07-17
uint32_t IC2Value,Frequency,miliseconds; float DutyCycle; static void TIM2_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; TIM_ICInitTypeDef TIM_ICInitStructure; /* TIM2 clock enable */ RCC_AP...
Re: How to get 4 channel input capture values from stm32f407 ?
2019-07-17
It is 50hz signal, it is too slow.Should I increase the TIM_ICPrescaler ? Is it going to enough for getting correct value?
Re: How to get 4 channel input capture values from stm32f407 ?
2019-07-17
but when use different timer for example Tımer 3 , all values are incorrect. Tımer 2 is 32 bit timer and Tımer 3 is 16 bit. Is it about it?
Re: Starting of STEVAL-ISA147V3
2019-07-05
I have also same problem in my project.
Kudos from
User
Count
Legacy member
1
View all