2019-07-17 9:45 AM
I have this code that works and i can turn an LED on:
#include "stm32f10x.h"
void RCC_Init(void){
RCC->APB2ENR |= RCC_APB2ENR_IOPCEN;
}
void GPIO_Init(void){
GPIOC->CRH |= GPIO_CRH_CNF13_0 | GPIO_CRH_MODE13_0 | GPIO_CRH_MODE13_1;
}
int main(void){
RCC_Init();
GPIO_Init();
GPIOC->BSRR = GPIO_BSRR_BR13;
while(1){
}
return 0;
}but when i change my port it doesn't work:
#include "stm32f10x.h"
void RCC_Init(void){
RCC->APB2ENR |= RCC_APB2ENR_IOPAEN;
}
void GPIO_Init(void){
GPIOA->CRL |= GPIO_CRL_CNF7_0 | GPIO_CRL_MODE7_0 | GPIO_CRL_MODE7_1;
}
int main(void){
RCC_Init();
GPIO_Init();
GPIOA->BSRR = GPIO_BSRR_BS7;
while(1){
}
return 0;
}Based on the datasheet and the clock table shown, it should work. Can anyone point out the problem to me?
Solved! Go to Solution.
2019-07-17 1:16 PM
Okay I found out what the problem was. The default value of the register is not 0x00000000 by default; It is 0x44444444. So, in other words, for me to implement this table:
What I was missing is shifting two zeros to CNF[1:0]. To do this I must write the following code:
void GPIO_Init(void){
GPIOA->CRL |= GPIO_CRL_MODE7; // Output 50MHz
GPIOA->CRL &= ~(GPIO_CRL_CNF7); // Set CNF[1:0] to 00
}Instead of this:
void GPIO_Init(void){
GPIOA->CRL |= GPIO_CRL_MODE7; // Output 50MHz
}Thanks for your answer anyways mate.
2019-07-17 12:15 PM
If I understand it correctly, you set the pin to General Purpose Output, Open Drain. Is this what you intended? Why do you then *set* the pin's output register? How are the LEDs connected, exactly?
I am not very familiar with the 'F1xx family.
JW
2019-07-17 1:16 PM
Okay I found out what the problem was. The default value of the register is not 0x00000000 by default; It is 0x44444444. So, in other words, for me to implement this table:
What I was missing is shifting two zeros to CNF[1:0]. To do this I must write the following code:
void GPIO_Init(void){
GPIOA->CRL |= GPIO_CRL_MODE7; // Output 50MHz
GPIOA->CRL &= ~(GPIO_CRL_CNF7); // Set CNF[1:0] to 00
}Instead of this:
void GPIO_Init(void){
GPIOA->CRL |= GPIO_CRL_MODE7; // Output 50MHz
}Thanks for your answer anyways mate.