STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

error on address

I'm trying to use the LCD screen in STM32N6570DK, but it has an error like this`Break at address "0x18003a1a" with no debug information available, or outside of program code.`. But when I tried to view the vector table generated by disassembly, It wi...

creeper_0-1746500539292.png
creeper by Associate II
  • 1235 Views
  • 2 replies
  • 0 kudos

STM32H563 DMA Issue

Hi, I'm trying to implement read ADC1 value triggered with TIM6 then write it via DMA(GPDMA1 CH0). I created CubeMx project and generate code accordingly (Using LL driver). But I can't enabled DMA channel. Is there any code example about it? 

RTC calib register values

I am trying to calibrate 512Hz RTC  to 1ppm or <1ppm. Desired Frequency = 512HzAverage Frequency Obtained is = 512.0073HzWhat should be the value of CALP and CALM ??? (I used the CALP = 0 and CALM = 15, but still the ppm that I obtained is ~14) Could...

J_Thomas by Associate II
  • 474 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F446RET6 DAC to generate "an ideal square wave"

Hi,   I want to generate a bipolar square wave with a pulse width of 100us per phase using the DAC in STM32F446RET6.        But when I measured the DAC output (PA4), I found that the DAC output was not an ideal square wave, but a trapezoidal shape w...

Junzhe_2-1747249767726.png
Junzhe by Associate II
  • 4862 Views
  • 13 replies
  • 6 kudos

How to set this RCC_RDCR reigster for bootrom?

MCU: STM32N6Register: RCC reset duration control register (RCC_RDCR)Bits 27:24 EADLY[3:0]: External access delayThe bit field is security-protected by the 1 bit. Set and reset by software.Time to wait before the BOOTROM performs any external device a...

Resolved! STM32F7 USB Device Not Recognized as Virtual COM Port (VCP)

Hello everyone,I’m working on an STM32F7 project where I’m trying to establish USB communication between my STM32F746 Discovery board and a PC. I am really new at this really first time. I have configured the board for USB_OTG_FS in STM32CubeMX, and ...

Rlakos by Associate II
  • 6603 Views
  • 8 replies
  • 5 kudos

Resolved! Vector address & interrupt handler

Hello at everyone,I setup on CUBE Ide on STM32C011 mcu without the configurator TIMER1 and I would to manage it on update interrupt, but I have not the stm32c0xx_it.c file that would contain the irqHandler routines.In this case, how the compiler iden...

VSimo.18 by Associate II
  • 2211 Views
  • 6 replies
  • 0 kudos

Resolved! STM32G0B1CCT6 have FDCAN1 or FDCAN2

My question is that stm32g0b1cct6 have fdcan2 or not because i getting confuse i read many document and reference some are said that stm32g0b1cct6 is low budget mcu and its have only fdcan1 not fdcan2 . so dear support team plz response fast regard V...

Vika43121_0-1747289760178.png

F446 Bitwise operator MODER & PUPDR

Hello.. i m programming F446 using registers, and i found from F446 reference manual to configure PA1 as both input and pull-down mode. i don't understand , can anyone advise how could1. MODER &= ~(3<<2)  is to set MODER1 as 00 input? 2. PUPDR |=  (1...