User Activity

Is it possible for BissC absolute encoder to communicate with STM32F401Re via SPI? Or can it be with MAX485 module as in the ardunio example in the link below?  https://protonestiot.medium.com/communication-between-24-bit-rotary-encoder-working-with-...
I am working with STM32F401RE and IHM04A1 driver board. There is timer1 channel 3 in EN-A (PA10) for IN1A and IN2A. However, there is no timer channel in EN-B which should be used for IN1B and IN2B. What should I do for the timer in EN-B, that is, PC...