2025-01-05 11:45 AM - last edited on 2025-01-06 2:36 AM by Andrew Neil
I am working with STM32F401RE and IHM04A1 driver board. There is timer1 channel 3 in EN-A (PA10) for IN1A and IN2A. However, there is no timer channel in EN-B which should be used for IN1B and IN2B. What should I do for the timer in EN-B, that is, PC1?
2025-01-06 12:53 AM
Welcome @aknaydn, to the community!
EN-A is not controlled via a timer channel, but via a normal GPIO. For bridge 1, this is EN-A, which is controlled via PA10; for bridge 2, this is EN-B, which is connected to PC1.
Hope that helps?
Regards
/Peter
2025-01-06 2:08 AM
Thanks for your reply. PA10 used for En-A from STM32F401 kit can be operated as Pwm with the 3rd channel of Timer 1, but PC1 used for En-B does not have a timer function. What should I do to use En-B as a timer with its channel?
2025-01-06 3:41 AM - edited 2025-01-06 3:42 AM
Pin PA10 of the STM32F401RE has many functions and can also work as a timer output. But how did you come up with the idea of controlling the (global) enable pin of a motor full bridge via PWM? As mentioned, this is done by switching a GPIO (slowly) on or off, as can also be found as:
in the X-CUBE-SPN4 example software.
2025-01-06 3:41 AM
Pin PA10 of the STM32F401RE has many functions and can also work as a timer output. But how did you come up with the idea of controlling the (global) enable pin of a motor full bridge via PWM? As mentioned, this is done by switching a GPIO (slowly) on or off, as can also be found as:
in the X-CUBE-SPN4 example software.