STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

extra byte in front of USART buffer received with DMA

I have inherited code that received 1400 bytes over a 2mbps serial link. I've increased that to 1892 bytes and on occasion (not always, but frequently enough to be annoying) I receive my buffer "shifted" by one byte and a garbage byte for byte 0 in t...

RPhil by Associate
  • 2061 Views
  • 3 replies
  • 0 kudos

DMA stop working after a sucessful receiving data USART.

In a noisy media, I need to receive 10bytes with DMA (about 1Mb). I have set the DMA and its interrupt as shown below:void DMA_Configuration(void) { DMA_InitTypeDef DMA_InitStructure;   RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);      ...

parisa by Senior
  • 3700 Views
  • 9 replies
  • 0 kudos

IoTA2+F413H

Hi everyone!i have an issue with communication! As shown below, when I press the green button I want to toggle led on the IoT board & when it’s the red I want to toggle WiFi ble led( I didn’t find an other user led)if i press the red button it works ...

idrissmc by Associate III
  • 1246 Views
  • 0 replies
  • 0 kudos

new STM32H7B3 and SRAM quantities

Hello,I have a doubt about the amount of SRAM available on the STM32H7B3.In the datasheet it is indicated 1184kB (setion embedded SRAM), but the linker script indicates 1024kB.In the datasheet, there is not much detail on this.My goal is to use for a...

PCu1 by Senior
  • 2018 Views
  • 4 replies
  • 0 kudos