STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0 CAN bus availability

Hi,The STM32G0 seems like a nice lineup for Mainstream MCUs.For my product the specs would fit quite nicely, but I would need CAN bus support.In several Presentations it is mentioned that some will support CAN FD (up to 2 instances), but I have not ...

stratom by Associate III
  • 7320 Views
  • 7 replies
  • 0 kudos

stm32f302 ADC capture influences input signal

I'm testing stm32f302 ADC capture with DMA transfer, but get some strange issues.I set the ADC1 to capture single channel AIN2(PA1) in continuous and DMA mode at 72MHz and 1.5 sample cycles. Set the DAC1 output a fixed voltage of 2048 with VDDA = 3.3...

0690X00000DYVf0QAH.jpg 0690X00000DYVfKQAX.jpg 0690X00000DYVfUQAX.jpg
YDong.11 by Associate II
  • 2788 Views
  • 7 replies
  • 0 kudos

STM32L4+ power scheme design while working at 1.8v

Hello, I will use STM32L4R9AI in a battery powered design with PSRAM that powered at 1.8v and flash memory that can work at wider voltage range (in addition to DSI display, RTC, ADC, DAC, USB, I2C) so my power scheme is as following:MCU:VDD : 1.8vVDD...

Hard Fault when calling the HAL_TIM_Encoder_Start_DMA function on the STM32F103C8T6 microcontroller. Can I fix it?

 HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(...

AndrewCh by Associate
  • 1832 Views
  • 4 replies
  • 1 kudos

Cube External Memory question

Hi everyone,I have recently starting becoming familiar with the M-Cortex structure and instruction set ( I was raised on Atmel MCUs in school and this is my first time working with M-Cortex and .thumb instructions) I am trying to learn as much as I c...

belair55 by Associate III
  • 1235 Views
  • 1 replies
  • 0 kudos

I2S DMA Complete transfer IRQ on circular mode

Hi, I'm using an audiocodec with a STM32F4011 through I2S interface. I configure I2S to transmit/receive in DMA mode and circular buffer. I need to get an ISR on HalfComplete and Complete transfer.HAL_I2SEx_TxRxHalfCpltCallback is fired on half compl...

leonardo by Associate III
  • 4772 Views
  • 9 replies
  • 0 kudos

STM32F205 USART2 Long zero level in tx transmitting

I use USART2 for connect whith gsm module.When trafic is big enough some byte in transmitting from cpu to modem can be corrupted.It may be happen one time in few minutes.I see corrupted byte by signal analisator. And the same corruption i see on the ...

0690X00000BuhXxQAJ.png