STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F101C8 Boot Loader reload?

Hello, New here. I am working with a piece of consumer electronics equipment that uses a STM32F101C8 processor. the customer was doing an update to this unit and in the middle of the update, pulled the USB plug out of his computer bricking the unit. ...

Resolved! Usage of ULPI & CANFD interfaces

I want to use the ULPI interface & both the CAN interface for my project But I see  For USB:   Pin No: 194     pin name: PB5     Module function :  USB_OTG_HS_ULPI_D7,   ONLY ONE PIN no other pins are there   For CAN   Pin No: 194,195    pin name: PB...

Meghna by Associate II
  • 2632 Views
  • 8 replies
  • 1 kudos

Resolved! Different Voltage Level on IO Pins

Hello, I am developing an application using STM32N657I have datasheet DS14791 Rev 4. There are pins for VDDIO2 to VDDIO5 and the datasheet implies that I can run the GPIO on an independent voltage supply. Chapter 5.3.17 even specifies low levels and ...

Panda by Associate III
  • 3860 Views
  • 7 replies
  • 2 kudos

SSD1963 Initialization

I am trying to get a 7" LCD to interface with a STM32F407VET6 microcontroller. I am using a display from winstar which the product number is WF70A2TIFGDBT0. The screen is 800x480 pixels and uses 8080 interface. The display uses a SSD1963 driver and I...

Resolved! Understanding Power Consumption using SMPS on STM32N6

I am unsure if I correctly understand the power consumption of the N6 Family. I want to supply the MCU with 1,8V and use the internal SMPS to supply Core with 0,81V.When it comes to designing the 1,8V voltage source, how much current do I have to exp...

Panda by Associate III
  • 2509 Views
  • 5 replies
  • 3 kudos

Resolved! Can't flash, debug or even erase STM32

Hi,I made some custom PCB's with a STM32L476RG. Here are some of the features:-USB-C connector (CC channel configured as device) with DM/DP routed to PA11/PA12.-Step down converter 5V (VBUS USB) to 3.3V (VCC for most components)-Tactile switches for ...

JonasHSLU by Associate III
  • 2885 Views
  • 7 replies
  • 1 kudos

STM32H7x3 ADC synchronous mode: clock ratio confusion

Board: NUCLEO-H723ZGMCU: STM32H723ZG (applies to others as well)Reference manual: RM0468 Rev. 3 Link  Dear community,I want to do a phase measurement of an approx. 75kHz analogue sine signal with respect to the HSE clock. For that purpose, I aim to t...

H7user_0-1747810477655.png
H7user by Associate
  • 885 Views
  • 0 replies
  • 0 kudos