User Activity

I have the following situation:I have a custom PCB with a 4 port HUB ic on it (TUSB8041IRGCR). The UFP of the hub is connected to  my phone and there are 4 DFP.My phone negotiates with the PD controller via CC lines about what voltage it wants when p...
How do i set the STUSB4700 so that it sources 12V 3A with the help of the GPIO pins (NO SOFTWARE)I read in the datasheet that there are several standard PDO configurations, selectable via GPIOs. But how? How do I say that i just want the PD controlle...