STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI communication between Slave and Master

This is my first post on this QnA section and i hope i would be getting help from the community. What i want to implement is a simple communication between 2 STM32 (both are F1 series in this case) using a SPI. Both the MCU are configured using CubeM...

0693W000000Vys5QAC.png 0693W000000VysAQAS.png

Resolved! Strange ST factory calibration on STM32f042k6 (ADC)

Hello,I'm trying to use temperature sensor and the internal voltage reference (VREFINT) of the STM32f042k6.Here is the extract form the datasheet (page 19/117) :When I measure these values, I don't have the same values than ST.For example, let's watc...

0693W000000VvHzQAK.png
ValentinG by Associate II
  • 1977 Views
  • 3 replies
  • 0 kudos

Better learning resources for Bluenrg-2?

Hey, folks.How are you people learning how to use the capabilities of your MCUs? In particular, I am trying to program a Bluenrg-2 board for a temperature control application. I would like to get better information on using the Multi-Function Timer...

BBeau by Associate
  • 881 Views
  • 0 replies
  • 0 kudos

AES-CBC(128 bit) Encryption for STM32H750VB IC

I am using STM32h750VB for a Project. I need to use AES -CBC Mode of Encryption.I have downloaded the cube-cryptolib and when I searched for the crypto code of my IC, I found that the AES CBC code is available for STM32H743ZI-Nucleo..Can i use the sa...

What's the bXCAN RXD recessive signal on STM32L476?

I'm reading RM0351 for STM32L476, "To be synchronized the hardware has to monitor a sequence of 11 consecutive recessive bits on the CAN RX signal." Is RX recessive bit a digital high or low signal? I couldn't find the info on the datasheet which onl...

ANguy.1 by Associate II
  • 1183 Views
  • 1 replies
  • 0 kudos

My data are being send in loop despite the datas are ACK.

static void FDCAN_Config(void) { FDCAN_FilterTypeDef sFilterConfig;   hfdcan.Instance = FDCAN2; hfdcan.Init.FrameFormat = FDCAN_FRAME_CLASSIC; hfdcan.Init.Mode = FDCAN_MODE_NORMAL; hfdcan.Init.AutoRetransmission = ENABLE; hfdcan.Init.TransmitPa...

SBACO by Associate III
  • 3556 Views
  • 8 replies
  • 0 kudos