Skip to main content
FFern.1463
Visitor II
Nov 21, 2019 2:43 PM UTC
Question

I'm monitorating heart rate by the MAX30100(https://img.filipeflop.com/files/download/Datasheet_MAX30100.pdf) using the MCU STM32F4. I'm trying read the IR and RED data from the FIFO, but all returns are **ZERO**.

I'm monitorating heart rate by the MAX30100(https://img.filipeflop.com/files/download/Datasheet_MAX30100.pdf) using the MCU STM32F4. I'm trying read the IR and RED data from the FIFO, but all returns are **ZERO**. The method `MAX30100_Get_Num_Samples()` returns **8**. I modeled the code using the pseudo code from datasheet of MAX30100. I tried several solutions for my problem but doesn't work. I dont know if i'm following the right way to get data from the FIFO. My code:

  I2C_HandleTypeDef hi2c3; //i2c used

  uint16_t RED[50] = {0}, IR[50] = {0}; //buffers for RED and IR

  uint8_t buffOximeter[5];

  char buffer[32];

  int main(void)

  {

   HAL_Init();

   SystemClock_Config();

   MX_GPIO_Init();

   MX_I2C3_Init();

   MX_USB_DEVICE_Init();

   MAX30100_Init();

   while (1)

   {

  uint8_t numSamples = MAX30100_Get_Num_Samples();

  MAX30100_Read_HeartBeat(numSamples);

  for(int i = 0; i < numSamples; i++)

  {

  sprintf(buffer, "Amostra %d: %d / %d\n\r", i , IR[i], RED[i]);

  CDC_Transmit_FS((char*)buffer, 50);

  }

   }

  }

  static void MX_I2C3_Init(void)

  {

   hi2c3.Instance = I2C3;

   hi2c3.Init.ClockSpeed = 400000;

   hi2c3.Init.DutyCycle = I2C_DUTYCYCLE_2;

   hi2c3.Init.OwnAddress1 = 0;

   hi2c3.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;

   hi2c3.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;

   hi2c3.Init.OwnAddress2 = 0;

   hi2c3.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;

   hi2c3.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;

   if (HAL_I2C_Init(&hi2c3) != HAL_OK)

   {

    Error_Handler();

   }

  }

  void MAX30100_Init(void)

  {

  HAL_I2C_Mem_Write(&hi2c3,0xAE,0x06,1,0x02,1,1000); //set heart rate mode

  HAL_I2C_Mem_Write(&hi2c3,0xAE,0x09,1,0xFF,1,1000); //i50 ledCurrent

  uint8_t sr = 0x01, pw = 0x3;

  HAL_I2C_Mem_Write(&hi2c3,0xAE,0x07,1,(sr<<2)|pw,1,1000); //sr100, pw1600

  HAL_Delay(50);

  }

  void MAX30100_Read_HeartBeat(uint8_t num)

  {

  for(int i=0;i<num;i++)

    {

  HAL_I2C_Master_Transmit(&hi2c3,0x57,0xAE,1,1000); //adress + write mode

  HAL_I2C_Master_Transmit(&hi2c3,0x57,0x02,1,1000); //send fifo_wr_ptr

  HAL_I2C_Master_Transmit(&hi2c3,0x57,0xAF,1,1000); //adress + read mode

  uint8_t data;

  HAL_I2C_Master_Receive(&hi2c3,0x57,&data,1,1000); //read fifo_wr_ptr

  HAL_Delay(100);  //STOP

  HAL_I2C_Master_Transmit(&hi2c3,0x57,0xAE,1,1000); //adress + write mode

  HAL_I2C_Master_Transmit(&hi2c3,0x57,0x05,1,1000); //send adress fifo data

  HAL_I2C_Master_Transmit(&hi2c3,0x57,0xAF,1,1000); //adress + read mode

  HAL_I2C_Mem_Read(&hi2c3,0x57,0x05,1,&buffOximeter,4,1000); //read fifo data

  IR[i] = (buffOximeter[0] << 8) | buffOximeter[1];

  RED[i] = (buffOximeter[2] << 8) | buffOximeter[3];

  HAL_Delay(100);                  //STOP

  HAL_I2C_Master_Transmit(&hi2c3,0x57,0xAE,1,1000); //adress + write mode

  HAL_I2C_Master_Transmit(&hi2c3,0x57,0x04,1,1000); //send adress fifo_rd_ptr

  HAL_Delay(100);

  }

  }

  int MAX30100_Get_Num_Samples(void)

  {

  uint8_t wrPtr, rdPtr;

  HAL_I2C_Mem_Read(&hi2c3,0x57,0x02,1,&wrPtr,1,1000);

  HAL_Delay(50);

  HAL_I2C_Mem_Read(&hi2c3,0x57,0x04,1,&rdPtr,1,1000);

  HAL_Delay(50);

    return (abs( 16 + wrPtr - rdPtr ) % 16);

  }

This topic has been closed for replies.

4 replies

Eleon BORLINI
ST Employee
Nov 21, 2019 3:14 PM UTC

Hi @FFern.1463​ , I suggest you to post the same question on the STM32 community page and/or on Maxim Q&A page, being the MAX30100 a Maxim sensor. Regards

Tesla DeLorean
Guru
Nov 21, 2019 10:49 PM UTC

What kind of forum software are you running? Just move posts to the appropriate sub-forum..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Amel NASRI
ST Technical Moderator
Nov 22, 2019 11:15 AM UTC

It is just a matter of editing tags (topics), I did it.

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.