User Activity

Hi,I'm wondering if a FSMC access interruptable? in another word, do I have to disable interrupt before accessing to the external memory with FSMC, then recover the interrupt status after? Or just use it as it is a internal memory, access it freely? ...
Posted on December 29, 2017 at 10:16I got a Nucleo F302R8 on hand, but now a STM8S003F3 is used on my project, i'm wondering if the STLINK on the Nucleo board can be used to debug the STM8S processor? and how should they be connected?Any comments ar...